AKD Capture Engine Configuration
The AKD capture engine provides a broad range of capabilities for configuration of the capture events.
- It is capable of configuring preconditions to allow the application programmer to specify sequential events or conditions that must be met before the capture event can be triggered.
- The capture Engine in the AKD is configured with SDO #0x3460 (subindexes 1 to 10).
- The AKD supports two capture engines (0 and 1); the application programmer must configure the desired engine.
|
Sub Index # |
Function |
|---|---|
|
1 |
Trigger for capture engine 0. |
|
2 |
Trigger for capture engine 1. |
|
3 |
Mode for capture engine 0. |
|
4 |
Mode for capture engine 1. |
|
5 |
Capture Event for capture engine 0. |
|
6 |
Capture Event for capture engine 1. |
|
7 |
Precondition edge for capture engine 0. |
|
8 |
Precondition edge for capture engine 1. |
|
9 |
Preselect for capture engine 0. |
|
10 |
Preselect for capture engine 1. |
AKD Configuration Parameters
These are the configuration parameters for the AKD capture engines.
See either CAP0.PRESELECT or CAP1.PRESELECT.
|
Parameter |
Description |
|---|---|
|
Capture Edge |
Programmed in the MC_Reference function block. |
|
Capture Event SDO object #0x3460 subindex engine 0 = 5/engine 1 = 6 |
|
|
Capture Mode SDO object #0x3460 subindex 3/4 |
|
|
Capture Precondition Edge SDO object #0x3460, subindex 7/8 |
|
|
Capture Preselect SDO object #0x3460 subindex 9/10 |
|
|
Capture Trigger SDO object #0x3460 subindex 1/2 |
|