Use HTTP Commands to Access the Control
HTTP commands can be used to get information directly from the controller.
HTTP over standard Ethernet TCP/IP is supported with Standard TCP connection, error checking, re-transmit, etc.
HTTP commands can be used to get information directly from the controller.
HTTP over standard Ethernet TCP/IP is supported with Standard TCP connection, error checking, re-transmit, etc.
|
See Kollmorgen Documentation Legal Information for legal ownership. |
|