EtherCAT Network Security Verification and Monitoring
KAS provides EtherCAT device verification and communication-monitoring capabilities that:
- Help detect unexpected or unintended changes to the configured EtherCAT network.
- Identify communication conditions that can affect network integrity or operation.
The KAS controller acts as the EtherCAT MainDevice.
During Startup and operation, the MainDevice uses information reported by the:
- Connected EtherCAT SubDevices.
- Configured EtherCAT network.
- EtherCAT communication diagnostics to verify devices and monitor network operation.
EtherCAT Security Profile
The EtherCAT Technology Group (ETG) defines EtherCAT cybersecurity measures in the ETG.1800 EtherCAT Security Profile.
- The profile provides a structured basis for selecting, implementing, and assessing appropriate EtherCAT security measures.
- Part 2 of the profile describes cybersecurity measures based on existing EtherCAT functionality and related process-management measures.
See these sites for information about EtherCAT cybersecurity and the related ETG measures:
-
-
- The EtherCAT capabilities description in this section supports applicable measures in the ETG.1800 EtherCAT Security Profile.
- They do not, by themselves:
- Provide cryptographic device authentication.
- Prevent physical manipulation of the EtherCAT network.
- Independently establish conformity with the EU Cyber Resilience Act (CRA).