AXIS_REF Structure
The PLCopen specification indicates a Structure used for identifying the axis at a function block input.
AXIS_REF contains these members:
|
Member |
Type |
Description |
|---|---|---|
|
AXIS_NUM |
INT |
The axis number. |
|
AXIS_ENGINE |
UINT |
Reserved. Do not modify this variable or rely on its value. |
See Change a PLCopen Axis about Axis Number.
You have to create and initialize this data structure in your application.