PLCopen
Kollmorgen Automation Suite supports the International
- The PLCopen international standard was created to obtain uniformity of motion function blocks and motion startup between machine control products.
- Users familiar with PLCopen are automatically familiar with PLCopen inside the KAS-IDE.
- The PLCopen function blocks for Motion Control, is based on the IEC 61131-3 Function Blocks (POU) concept with these factors in consideration:
- Completeness
- Consistency - conforming to the IEC 61131-3 standard
- Efficiency - in the number of function blocks, for efficiency in design (and understanding)
- Flexibility - future extensions / range of applications
- Simplicity - ease of use for the application program builder and installation & maintenance
- Universality - hardware independent
KAS supports PLCopen motion in these program formats: FBD, FFLD, IL, SFC, and ST.
- PLCopen blocks in KAS start with MC (e.g., MC_MoveAbsolute).
- MC blocks are an alternative to using the ML Motion function blocks (e.g., MLAxisAbs) and associated Pipe Networks in many applications.
- Using MC Motion function blocks does not require a separate motion editor.