Functions (POU)
IEC has defined standard functions and also allows you to create your own functions (called user-defined functions). Typically, functions take several inputs and return a single output as the result of processing.
- Standard functions are for example ADD (addition), ABS (absolute), SIN (sine), COS (cosine), GT (Greater Than),….
- User-defined functions, as in this example, can be used repeatedly once defined.
FUNCTION SIMPLE_FUN : REAL VAR_INPUT A, B : REAL; C : REAL := 1.0; END_VAR SIMPLE_FUN := A*B/C; END FUNCTION