Add and Configure a Servo Drive

  1. In the Project Explorer, right-click the EtherCAT node to open the menu.
  2. Select the Add Device... command.
    This option is disabled when you are connected to the controller and an application is running.
  3. Select the specific servo drive model to add. (Figure 1)
  4. Figure 1: EtherCAT Device Selector dialog box


      • When choosing any of the Kollmorgen Servo Drives, be sure to select the newest revision.
      • Older revisions may show in the list of options, but they may not be feature complete.
      • If a specific revision number is required, select it from the drop-down list in the Revision column.
      • The default selection is the highest revision number.

  5. Click OK to save the changes or selections and close the dialog box.
    See Kollmorgen Servo Drives.
  6. In the Project Explorer, right-click the device node and select the Rename command. (Figure 2)
  7. Figure 2: Rename

  8. Define the name for the new device.
    The name is limited to 10 characters and can only include letters, numbers, and underscores. (Figure 3)
  9. Figure 3: Rename dialog box

  10. Click OK.
  11. Continue with Add and Configure Third-party EtherCAT Devices.

When an Kollmorgen AKD Series Servo Drive is added to the project tree, it must be mapped to a physical drive.


  • An alternative method to add a drive is to rely on the auto scan feature.