Configure Custom Project Settings

The KAS Runtime is used to modify specific configurations within a user's application without needing to access the KAS-IDE, recompile and re-downloading the project file to the controller.

  • This functionality streamlines configuration management, particularly for customers commissioning multiple machines using a single KAS project file.
  • This custom project configuration feature supports modifying the Server IP addresses of the EtherNet/IP IO Scanner (Client) defined in the KAS project.

Procedure

  1. Create the controller settings file.
    1. Create a text file named controller_settings.xml with this content:
    2. <?xml version="1.0" encoding="utf-8"?>
      <KasControllerConfig xmlns="KasControllerConfig">
          <IpAddrMapping>
              <IpAddrAlias alias="1.1.1.1" canonical="192.168.1.91" />
              <IpAddrAlias alias="2.2.2.2" canonical="192.168.1.177" />
              <IpAddrAlias alias="3.3.3.3" canonical="192.168.1.213" />
          </IpAddrMapping>
      </KasControllerConfig>
      

      • The alias IP addresses must match exactly the Server IP Address specified in the KAS project under the Fieldbus Editor > EtherNet/IP IO Scanner (Client) -> Server nodes.

    3. Replace the canonical IP addresses in the configuration file with the actual EtherNet/IP addresses of your adapter controllers.
  2. Upload the file to the scanner controller.
    1. Open a command prompt.
    2. Using curl, run these commands to upload the file:
      1. curl.exe -k -X POST -d "username=administrator" -d "password==<<administrator_account_password>>" -G https://(IP_Address)/authorize/login -c cookie.txt
      2. curl.exe -k -F "sendfile=@<<controller_settings.xml file path>>" -F "filename=controller_settings.xml" https://(IP_Address)/userfiles -b cookie.txt

        • Replace the (IP_Address) with the actual IP address of your scanner controller (PCMM2G).
          • Example:
            curl.exe -k -F "sendfile=@<<C:\tmp\controller_settings.xml" -F "filename=controller_settings.xml" https://192.168.0.10/userfiles -b cookie.txt
        • Replace <<administrator_account_password>> with the actual password of the controller Web server.
        • See HTTP Commands for User Data File Management.
  3. Verify the file upload.
    1. Open a web browser and navigate to https://(IP_Address).
    2. Navigate to: KAS Application > User Data page.
    3. Locate the controller_settings.xml file and click the Download () icon next to it. (Figure 1)
    4. Once the file is downloaded, open it and verify that its contents are correct and as expected.
    5. Figure 1: controller_settings.xml file

  4. Configure the KAS project.
    1. In the KAS-IDE, open the KAS application project.
    2. Stop the project if it is currently running.
    3. In the Project Explorer, double-click Fieldbus to open the FieldBus Editor.
    4. Under the Server nodes, update the IP address to match the alias values from the XML file. (Figure 2)
    5. Figure 2: Alias IP address

  5. Verify the operation.
    1. Compile and download the project to the controller.
    2. Start the project and wait for the application to fully initialize.
    3. Confirm that all EtherNet/IP I/O Scanners are operating correctly and communicating as expected.

See Also

EtherNet/IP IO Scanner (Client)