Pipe Network Functions for the PLC
After creating the Pipe Network, the complete project must be compiled before using the Pipe Network in PLC Programs.
- Compiling creates a list of Functions used in the PLC Program.
- These Functions simplify programming by combining the same function block for all axes in the Pipe Network:
|
Pipe Network Function |
Included Function Blocks (for 2 axis system) |
|---|---|
|
MLPipeAct( PipeAXIS1 ); MLPipeAct( PipeAXIS2 ); |
|
|
MLCNVConnect( CNV1, AXIS1 ); MLCNVConnect( CNV2, AXIS2 ); |
|
|
MLAxisPower( AXIS1 ); MLAxisPower( AXIS2 ); |
|
|
MLAxisPowerOFF( AXIS1 ); MLAxisPowerOFF( AXIS2 ); |
|
|
MLPipeDeact( PipeAXIS1 ); MLPipeDeact( PipeAXIS2 ); |
See click here... about constant definitions related to Pipe Network.
-
-
To see how these functions are used, open a project, go to Project Explorer, right-click on PipeNetwork and select the Show compiled Code command.