Analog I/O Parameters
AKT2G Input Terminals
The offset and gain is applied to calculate the value converted from the analog input:
PLC Variable Value = Analog to Digital Converter Value x Gain + Offset
Where the Gain and Offset are configured from the terminal’s I/O tab.
See E-Bus Analog I/O Data Representation for more information.
AKT2G Output Terminals
The offset and gain is applied to calculate the value to be converted to the analog output:
Digital to Analog Converter Value = PLC Variable Value x Gain + Offset
Where the Gain and Offset are configured from the terminal’s I/O tab.
See E-Bus Analog I/O Data Representation for more information.
AKT Input Terminals
The process data that are transferred to the Bus Coupler are calculated using these equations:
Ya = ( Ba + XADC ) x Aa
Yout = Bw + (( Aw + Ah ) x Ya )
With these parameters:
|
Parameter |
Description |
|---|---|
|
XADC |
Output values of the Analog Input Modules A/D converter. |
|
Yout |
Process data to the controller. |
|
Ba , Aa |
Manufacturer offset and gain compensation ‡. |
|
Ah |
Manufacturer scaling: default gain ‡. |
|
Bw , Aw |
User scaling: Offset and Gain as set in the Analog Input Properties. |
‡ For the thermocouple input terminals, AKT-AN-200-000 and AKT-AN-400-000, the manufacturer default gain is 160.
For all other supported terminals, the manufacturer default gain is 1.
The manufacturer default offset is 0 (zero) for all supported terminals.
Figure 1: Analog Input Properties
AKT Output Terminals
The process data that are transferred to the Bus Coupler from the controller are calculated using these equations:
Y2 = Bw + (( Aw x Ah ) x X )
Ydac = Y2 x Aa + Ba
With these parameters:
|
Parameter |
Description |
|---|---|
|
X |
Controller Process data. |
|
Ydac |
Controller data to analog output module D/A converter. |
|
Ba , Aa |
Manufacturer offset and gain compensation ‡. |
|
Ah |
Manufacturer scaling: default gain ‡. |
|
Bw , Aw |
User scaling: offset and gain as set in the Analog Output Properties. |
‡ The manufacturer default offset is zero for all supported terminals.
The manufacturer default gain is 1 for all supported terminals.