PDO Restrictions and Compiler Errors
- Restrictions for AKD Devices
- Restrictions for AKD2G Devices
- Restrictions for Kollmorgen Essentials Drive and KLD Devices
- Restrictions for All Other Devices
Restrictions for AKD Devices
The KAS-IDE compiler enforces these restrictions to the editable PDOs for AKD devices:
- The maximum byte count for the content of an individual PDO (both selected and unselected) is 8 bytes.
- The PDO content Size field is highlighted in red if the Editable PDO content size is greater than 8 bytes.
- The total maximum byte count for the content of all Tx PDOs (both selected and unselected) is 32 bytes.
- The total maximum byte count for the content of all Rx PDOs (both selected and unselected) depends upon the firmware.
Firmware Version
Byte Limit
Notes
v1-17 or later
32 bytes
This is the byte limit when the EtherCAT parameter ECAT.LEGACYREV is set to 0 (zero).
v1-16 or later
20 bytes
This is the byte limit when the EtherCAT parameter ECAT.LEGACYREV is set to 1.
v1-15 or earlier
20 bytes
- The total byte count for the content of all selected Tx PDOs must be even.
- This does not apply to AKD2G devices.
- The total byte count for the content of all selected Rx PDOs must be even.
- This does not apply to AKD2G devices.
-
- The object 0x00 can be used to pad the PDO to get the total byte count to an even value.
-
- Compiler errors are generated if these restrictions are not met.
These are example compiler errors:
In AKD_1, the size of Rx PDO 0x1600 is greater than the limit: 9 > 8
In AKD_1, the total byte count for all editable Rx PDOs is greater than the limit: 39 > 32
In AKD_1, the total byte count for all editable Rx PDOs that are assigned is not even: 29
Restrictions for AKD2G Devices
The KAS-IDE compiler enforces these restrictions to the editable PDOs for AKD2G devices:
- PDOs have a size constraint of 128 bytes per PDO.
- The total maximum byte count for the content of all Rx PDOs (both selected and unselected) is 512 bytes.
- [(128 per PDO) x 4 = 512 bytes].
- The total maximum byte count for the content of all Tx PDOs (both selected and unselected) is 512 bytes.
- [(128 per PDO) x 4 = 512 bytes].
- Based on the Sample Rate / Cycle Time, there is a limitation to the number of PDOobjects:
|
Sample Rate |
Cycle Time |
Max. PDOs |
|---|---|---|
|
4 kHz |
250 µs |
14 Rx, 14 Tx |
|
2 kHz |
>500 μs |
30 Rx, 30 Tx |
Restrictions for Kollmorgen Essentials Drive and KLD Devices
The KAS-IDE compiler enforces these restrictions to the editable PDOs for Kollmorgen Essentials Drive
- PDOs have a size constraint of 128 bytes per PDO.
- Rx PDOs
- The maximum number of Rx PDOs supported is 14.
- The total maximum byte count for the content of all Rx PDOs (both selected and unselected) is 512 bytes.
- [(128 per PDO) x 4 = 512 bytes].
- Tx PDOs
- The maximum number of Tx PDOs supported is 14.
- The total maximum byte count for the content of all Tx PDOs (both selected and unselected) is 512 bytes.
- [(128 per PDO) x 4 = 512 bytes].
Restrictions for All Other Devices
The KAS-IDE compiler enforces the following restriction to the editable PDOs for all devices:
- The maximum byte count for the content of an individual PDO (both selected and unselected) is 64 bytes.
- Compiler errors are generated if these restrictions are not met.
Example compiler error:
In Device_1, the size of Tx PDO 0x1A16 is greater than the limit: 66 > 64