Device Control

Start / Stop the Device

With the KAS-IDE

Start / stop the device with the buttons and .

With the KAS Runtime

In the KAS Runtime menu, click the start / stop command.

Start Device with the Run Time

Figure 1: Start Device with the KAS Runtime

Log Window

The Log window displays all run-time messages issued by the device or by the KAS Simulator when testing the application.

  • The log area of the KAS-IDE and the KAS Runtime Simulator are the same.
  • It contains the log messages as described in Information and Logs window.