KAS-IDE Runtime Compatibility

The KAS software includes two main software components, the KAS-IDE and the Runtime.

  • The KAS-IDE resides on your PC and the Runtime resides on the programmable automation controller (PCMM2G).
  • For optimum operation, the KAS-IDE installed and run on the PC must be compatible with the Runtime installed on the controller or programmable drive.

The KAS installer and controller Runtime contain the version information in the file name.

The version is determined by:

Version Source

Found From

Example

KAS-IDE, Controller, or Simulator

Help menu > About

Figure 1: Example: Product details - About Version

PCMM2G

Web server Settings Firmware tab

Figure 2: Example: PCMM2G Firmware version

The compatibility between the KAS-IDE and the Runtime is defined by matching the digits in the versions.

The KAS-IDE and Runtime use the same version scheme:

major . minor . micro . revision
  • If the KAS-IDE to Runtime major.minor is:
    • NOT equal, they are NOT compatible.
    • Is equal, but the micro is NOT equal, they are not 100% compatible.
  • If the KAS-IDE to Runtime major.minor.micro is equal, they are compatible.

Examples

IDE

Runtime

Compatible?

IDE to Runtime Connection

5.01.xx.xxxx

1.2.xx.xxxx

NO

No connection.

The KAS-IDE displays an error message.

5.01.0.xxxx

5.01.1.xxxx

YES*

Connection possible.

The KAS-IDE displays warning and requires user to click OK to continue.

5.01.0.xxxx

5.01.0.xxxx

YES

Normal connection.

5.01.0.30540

5.01.0.30540

YES

Normal connection.

*Not a recommended configuration.

  • The KAS-IDE operates but there can be different features available between the KAS-IDE and the Runtime.
  • It is recommended to upgrade either the KAS-IDE or the Runtime to matching versions.

Digital Signatures

The KAS-IDE Installer and the executables are digitally signed to protect the integrity of these files and identify the distributor of the software components.

The digital signature appears as part of the file properties.

Figure 3: Example: KAS Setup Properties Digital Signature