EtherCAT Devices Backup

The Backup operation discovers all devices on the EtherCAT network and stores the topology information, drive firmware files, and parameters.

Controller

Local Storage

PCMM2G

Controller flash memory.

Required Items

These items are required before starting a backup of the EtherCAT devices:

  • The Kollmorgen AKD Series Servo Drives firmware files package (you are prompted with the expected file).
    • The package is:
      • Included in the KAS software installation directory
        • Example: \Program Files (x86)\Kollmorgen\Kollmorgen Automation Suite {{kas.version}}\Astrolabe\DrivesFW.
        • Example: C:\Users\{user.name}\Local\Kollmorgen\Kollmorgen Automation Suite {{kas.version}}\Astrolabe\DrivesFw.
      • Available for download from Kollmorgen's AKD Series Servo Drives website.
  • PCMM2G requires a USB flash drive connected to the USB port.

Device Connection and Configuration

All EtherCAT network devices must be:

  • Connected to the controller.
  • Configured as necessary for machine operation.
  • A PLC application downloaded to the controller, containing the EtherCAT device map.

  • Verify the devices are in the order as expected.
    The topology information is stored in the backup and is used to check for identical topology during a restore function.
    The device order is not important.Example: An AKD can be anywhere in the EtherCAT topology but, for restore to occur, the devices must be in the same order as when backed up.

  • The PLC application cannot be running and the IDE must not be in Online Configuration Mode.
    Stop the PLC application or disable Online Configuration Mode before a Backup or Restore.

Modular EtherCAT

This procedure should be followed to backup EtherCAT devices when the modular EtherCAT feature is used to remove devices to create a machine variant.

See Modular EtherCAT Concept.

  1. Run the KAS application which sets up the correct EtherCAT topology for the machine variant.
  2. Stop the KAS application.

  • Do not power cycle or reboot the controller between Steps 2 and 3.
  1. Backup the EtherCAT devices.
    See Backup Procedure.

Backup Procedure

  1. On the Web server home page, click the Backup & Restore tab.
  2. On the Backup tab, click the Backup EtherCAT Devices button.
  3. The web server will ask you to choose one or more firmware package files and suggest the filename that matches the firmware version on your drives.

    • Selecting the firmware package files is a one-time event.
    • The controller remembers the selection for future backups. (Figure 1)

    Figure 1: Web server Backup


    • Kollmorgen servo drives have a firmware package file specific to its drive model and firmware version.
  4. Click the Continue Backup EtherCAT Devices button. (Figure 2)
    It will take a couple of minutes or longer, depending on the number of Kollmorgen servo drives present in the system.
  5. Figure 2: Web server Backup Continue

When the backup is complete, the Web server indicates whether the backup was successful.