Controller Error and Alarm Descriptions

When either Errors or Alarms occur, always check the controller log messages.

  • The controller continuously displays any error or alarm codes after booting and not in recovery mode.
  • Errors have a priority over Alarms.
    • Only one error or alarm code is displayed at a time.
    • The code with the highest priority is displayed until it is cleared.
  • The log messages provide more details about the failure and the history of events leading up to the failure.
    • Use the log messages to determine the specifics about the cause of the failure and correct the underlying problem.

Errors

 

 

 

 

 

 

 

 

 

 

Alarms

 

 

 

Errors


    • **In the How to Clear column:
      • HW indicates a reboot is required to clear the error or alarm.
      • SW indicates the error or alarm can be cleared from the web server.
      • APP indicates the error or alarm is automatically cleared when the application is restarted.


Code

Description

Cause

Remedy

How to Clear**

E01

PCMM2G:

  • After 20 seconds, the PLC application is stopped.
  • The CPU is throttled.
  • Critical temperature reached.
    • Critical temperature limit is 83 °C.

Controller temperature exceeds the safe operating temperature limit.

  • Power-off.
  • Check airflow and operating environment are within hardware specifications.
  • Allow unit to cool before power-on.
  • SW: 
    • PCMM2G

E02

Out of memory.

KAS Runtime is stopping.

Memory leak, memory corrupted, or hardware memory failure.

  • Power-off/on.
  • If the problem is recurrent, check the Release Notes for firmware updates.
  • If the problem persists, return the hardware for repair.

HW

E03

Fan failure.

CPU cooling fan is not able to operate properly.

  • Check temperature and monitor for High temp alarm (see A01).
  • Return the hardware for fan replacement.
  • SW: 
    • PCMM2G

E10

Firmware is corrupted.

Flash memory corrupted during firmware download or flash hardware failure.

  • Re-download firmware.
  • Boot into recovery mode, download firmware, and power-off/on.
    See Recover Using the Web server for more information.
  • If the problem persists, return the hardware for repair.

SW

E12

Not enough flash memory available.

Flash memory is full, unable to write to flash.

Clean-up the flash memory by removing log files, application programs, recipes, or other data files.

SW

E13

Out of NVRAM space to Retain Variables.

NVRAM is full.

Change application to reduce the amount of retained variables.

SW

E15

Cannot read / write files from/to a USB flash drive.

  • PLC function failures do not cause this error.
  • USB flash drive is not plugged in.
  • The file system is corrupt and cannot be mounted.
  1. Plug-in a valid USB flash drive.
  2. Reformat the USB flash drive using the Settings > USB Flash Drive > Format button.

SW

E16

Not enough space available on the USB flash drive.

  • USB flash drive is full, unable to write to the USB flash drive.
  • PLC function failures.
  • Clean-up the USB flash drive space by deleting files.
  • Reformat the USB flash drive using the Settings > USB Flash Drive > Format button.

SW

E17

Cannot connect to a shared directory.

  • Improper shared directory configuration on remote computer or the controller.
  • Improper permissions, access control, or security policy for computer’s share configuration.
  • Computer is not accessible via Ethernet network.
  • Verify the computer's shared directory is accessible.
  • Check and Apply the KAS Application > Shared Directory configuration.
  • Power-off/on the controller.

SW

E20

Runtime plug-in, process, thread or application failed to start.

  • KAS Runtime or application code failed to auto-start at boot.
  • Caused by either a high controller temperature at power up or a system error.
  1. Check the web server for other alarms or errors (e.g., temperature alerts) and resolve them.
  2. Power cycle the device.
  3. If E20 is still reported, reset to factory defaults.
  4. If the problem is recurrent, check the Release Notes for firmware updates.
  5. Download firmware.

HW

E21

Runtime process, thread, or driver failed to respond during operation.

  • KAS Runtime code failed during normal operation.
  • In extreme cases, the display may indicate that the controller failed at an early stage of the Boot Sequence.
  • Power-off/on.
  • If the problem is recurrent, check the Release Notes for firmware updates.

HW

E22

Fatal error in PLC program, application stopped.

Virtual machine failed to execute an instruction.

  • Check the PLC application code for programming errors that could cause a fatal execution error (e.g., divide by zero, array out of bound, etc.)
  • Check that the IDE and controller Runtime versions are compatible.
  • Re-compile the application, download, and re-start.

SW

E23

CPU is overloaded.

Either:

  • The motion engine did not complete.
  • The PLC program did not complete within the timeout period due to excessive CPU load.
  • Stop the application.
  • Power-off/on.
  • Reduce the sample rate, simplify the application, or reduce the application cycles and restart the application.
  • See CPU Overload (E23).

SW

E24

PLC application cannot be started

PLC application cannot be started because of an existing condition.

Possible reasons:

  • Maintenance operation is in progress.
  • Controller is in Online Configuration Mode.
  • AKD Restore failed.
  • The IDE version of the compiled PLC code and controller runtime version do not match.
  • Previous download failed.
  1. Check the controller web-server home page for any maintenance operation in-progress.
    Wait for the operation to finish.
  2. Connect to the controller with the IDE and disable Online Configuration Mode.
  3. Check the EtherCAT network topology by using the Scan network button in the web-server’s Restore tab.
    Correct the physical topology and re-execute an AKD-x restore.
  4. The IDE version (only major.minor.micro) should match with runtime version.
    To correct, install the correct version of IDE or Runtime.
  5. Connect the IDE and download application.

SW

E30

EtherCAT communication failure during operational mode.

Network communication error.

  • This is commonly caused by a loose or bad EtherCAT connection occurring after the network successfully starts up.
  • See the IDE Controller log for more information.
  • Read the AKD-x parameter ECAT.DIAG for more information on where in the EtherCAT network the issue may be occurring.
  • Check the EtherCAT network wiring and devices state.
  • Re-start the application.

SW

E31

EtherCAT communication failure during pre-op mode.

EtherCAT network operation failed due to a network communication error.

  • Check the EtherCAT network wiring and devices state.
  • Re-start the application.

SW

E32

EtherCAT communication failure during bootstrap mode.

EtherCAT network operation failed due to a network communication error.

  • Check the EtherCAT network wiring and devices state.
  • Re-start the application.

SW

E33

EtherCAT failed to initialize into operational mode.

EtherCAT network initialization failed.

  • This is commonly caused by the EtherCAT configuration in the project not matching the actual hardware.
  • See the IDE Controller log for more information.

SW

E34

EtherCAT failed to initialize into pre-op mode.

EtherCAT network initialization failed due to a network communication error.

  • Check the EtherCAT network wiring and devices state.
  • Re-start the application.

SW

E35

EtherCAT failed to initialize into bootstrap mode.

EtherCAT network initialization failed due to a network communication error.

  • Check the EtherCAT network wiring and devices state.
  • Re-start the application.

SW

E36

EtherCAT failed to discover the expected devices.

EtherCAT network discovery failed due to a mismatch between the discovered and expected devices.

  • Check the EtherCAT devices and wiring order.
  • Correct the device order wiring or re-scan the network, re-compile, and download the updated application.
  • Re-start the application.

SW

E37

EtherCAT failed to return to init state.

EtherCAT network initialization failed due to a network communication error.

  • Check the EtherCAT network wiring and devices state.
  • Re-start the application.

SW

E44

Software features license data is corrupted.

  • The detected software feature license stored on the controller is corrupted.
  • See the Controller logs for more information.

If Step 1 is not successful continue to Step 2.

  1. Power-off/on.
  2. If the problem is recurrent, check the Release Notes for firmware updates.
  3. If the problem persists, return the hardware for repair.

HW

E45

Axes count exceeded license limit.

The number of axes defined in the application is greater than the maximum number permitted by the controller model.

  • Review the system configuration.
    • Remove any axes beyond the licensed limit.
  • If additional axes are required, consider upgrading the controller to a higher-tier model (e.g., 8 axes to 24).
  • See Controllers for available models.

APP

E50

Backup to USB flash drive failed.

An unrecoverable error occurred during the backup operation.

  • Repeat the backup to USB flash drive operation.
  • If it fails again, replace the USB flash drive.

SW

E51

Restore from USB flash drive failed.

An unrecoverable error occurred during the restore operation.

Do not reboot the Controller!

  • Repeat the restore operation.
  • If it fails again, reset the Controller to factory defaults.
  • If the problem persists, return the hardware for repair.

SW

E52

USB flash drive Backup files are missing or corrupt.

The restore operation failed due to missing, incomplete, or corrupt files on the USB flash drive.

  • Perform a backup operation before the restore.
  • Use a USB flash drive with valid backup files.

SW

E60

PCMM2G only.

Inactive partition is corrupted.

PCMM2G only.

An unrecoverable error occurred when starting KAS Runtime on the inactive partition.

PCMM2G only.

These are the recovery steps.

If Step 1 is not successful, go to Step 2 and continue to Step 3 if needed.

  1. Re-download firmware.
  2. Boot into recovery mode, download firmware, and power-off/on.
    See Recover Using the Web server for more information.
  3. If the problem persists, return the hardware for repair.

See Booting the PCMM2G Controller for more information about partitions.

SW

Alarms


    • **In the How to Clear column:
      • HW indicates a reboot is required to clear the error or alarm.
      • SW indicates the error or alarm can be cleared from the web server.
      • APP indicates the error or alarm is automatically cleared when the application is restarted.


Code

Description

Cause

Remedy

How to Clear**

A01

High temperature exceeded.

CPU temperature near the safe operating temperature limit for:

  • PCMM2G = 78 °C

Check airflow and operating environment are within hardware specifications.

SW

A02

Low on memory.

Memory leak or corruption.

  • Power-off/on.
  • If the problem is recurrent, check the Release Notes for firmware updates.
  • If the problem persists, return the hardware for repair.

SW

A04

Low input voltage.

+24 volt input power is +19 volts or less.

Check power supply voltage and connection to the controller.

SW

A05

PCMM2G only.

The system time was not set on startup.

PCMM2G only.

  • Network Time Protocol (NTP) is disabled.
    • The time could not be retrieved at startup.
  • This is most likely caused by a dead or missing battery.

PCMM2G only.

Either:

  • Insert a good battery and set the time.
  • Enable NTP.
  • See Date/Time tab for more information.

SW

A12

Flash memory is low on free space.

Flash memory is almost full.

  • Clean-up the flash memory by removing log files, application programs, recipes, or other data files.
  • Reset to factory defaults.

SW

A21

Recoverable process or thread failed to respond during operation.

KAS non-runtime code failed during normal operation and was automatically restarted.

  • Power-off/on.
  • If the problem is recurrent, check the Release Notes for firmware updates.

SW

A23

CPU is heavily loaded.

CPU usage is too high for 5 (or more) seconds.

Reduce the sample rate, simplify the application, or reduce the application cycles.

SW

A30

EtherCAT missed a send frame during operation mode.

The EtherCAT master was unable to send a frame for one or more cycles.

Reduce the controller CPU load so it has enough Real-Time margin to send EtherCAT frames every cycle.

SW

A31

  • The slave EtherCAT device does not exist or cannot be physically reached due to connector and/or cable failure.
  • Slave hardware failure
  • Slave is still busy with a previous command and is not ready.
  • Check the EtherCAT cables and the connectors.
  • Check the EtherCAT devices for any device errors.

 

A38

EtherCAT missed a receive frame during operation mode.

See Actual Position Interpolation.

The EtherCAT master did not receive, or received too late, a frame for one or more cycles.

  • Read the AKD-x parameter ECAT.DIAG for more information on where in the EtherCAT network the issue may be occurring.
  • Check the EtherCAT network wiring and devices state.
  • Decrease the EtherCAT cycle rate.

SW

A40

Local digital IO missed a cyclic update.

Local digital IO was not updated during a cycle or the updates are no longer synchronous.

Reduce the sample rate, simplify the application, or reduce the application cycles.

SW

Actual Position Interpolation

  • If EtherCAT actual position data is missing due to a corrupted, late, or missing EtherCAT frame (A31 or A38), the controller interpolates the actual position data for servo axes, digitizing axes, and pipe network sampler blocks.
  • The interpolation reduces velocity discontinuities when the actual position data is used for camming and gearing.