Log Configuration tab
You can configure the log to filter the messages that are displayed.
Each Source can be set with its own Level.
Each message has one of these levels, with importance in descending order:
Error > Warning > Info > Debug
Choose the Appropriate Level
- When a level is set for a source, only messages with the same or higher importance are recorded.
- Example: If a source is set to WARNING, then all messages with levels WARNING, ERROR and CRITICAL are recorded (DEBUG and INFO messages are discarded).
- DEBUG is the most verbose and ERROR is the least verbose level.
- Filtering is quicker with less verbose levels because of the number of messages.
-
-
Critical messages are always recorded.
The Critical level is not visible.
Source
|
Source |
Apply to... |
|---|---|
|
Controller |
For the KAS Runtime items: Drivers, IOEngine, SinopEngine, etc. |
|
Drive |
Messages from Kollmorgen drives. |
|
EtherCAT |
For all kinds of EtherCAT items: Motion bus, I/Os |
|
IDE |
Win32 applications:
|
|
Motion |
Messages coming from the Motion engines:
|
|
PLC |
For application engineers to create a custom log within the PLC programs. See Printf Function. |
|
System |
For common API and libraries. Includes messages issued from the operating system. |
Level
|
Level |
Icon |
Description |
|---|---|---|
|
CRITICAL |
|
|
|
DEBUG |
|
|
|
ERROR |
|
The application does not behave as expected but the processes remain stable. |
|
INFO |
|
|
|
WARNING |
|
|