Web server Home page
To access the KAS Web server home page, enter the controller's IP address.
This page provides an overview of the device including:
- Manufacturer
- CPU Speed
- CPU Cores
- Model Name and Number
- See Controllers for the model name and number.
- Serial Number
- CPU Serial Number
- Hardware Revision
- TCP/IP MAC Address: A unique value associated with the TCP/IP network adapter that uniquely identifies the adapter on a LAN.
- EtherCAT MAC Address: A unique value associated with the EtherCAT network adapter that uniquely identifies the adapter on an EtherCAT network.
- Axis Count
- See Controllers for the motion axes count supported by each controller model.