Map Variables to the Control Panel
To link your Control panel with the PLC programs, some controls contain a property called Variable symbol. (Figure 1)
Figure 1: Map variables to a Control Panel control
Procedure
- Select the variable in the Dictionary toolbox.
- Move it to the control to be linked in the Control panel editor using drag-and-drop. (Figure 2)

Figure 2: Map Variables to a Control Panel Control in the Graphical Editor
The Variable symbol is automatically updated in the Properties tab.
-
-
A warning is generated when the program is compiled if the control is mapped to a variable not in the Dictionary.
Double-click the warning to highlight the control object and open the editor so the variable can be defined.