Use the Kollmorgen Visualization Builder (KVB)

To work with Kollmorgen Visualization Builder:

  1. Tag the PLC variables to export and map with the HMI (see Map Variables to HMI for more information).
  2. Compile your project to generate the Modbus mapping file.
  3. Create a KVB project 1 in the KAS-IDE and open it.
  4. Design the HMI Panel with KVB .
  5. Save and close KVB.

    • Important! Be sure to use Save and not Save As.
      The KVB is self-contained within the KAS archive and the Save As function moves the KVB out of the archive.

  6. Save your KAS project.

  • Be aware that as soon as you change the PLC variables exported for the HMI, the mapping file must be re-imported in Kollmorgen Visualization Builder to have an up-to-date version.

Related Documents

For further information on Kollmorgen Visualization Builder, see this documentation:

KVB Manuals

Description

Quick Start Guide

The Quick Start covers these important points to:

  • Install and use Kollmorgen Visualization Builder.
  • Configure HMI Panels and PC operated control applications.

User Manual

Contains all the content to help with Kollmorgen Visualization Builder.

Concept Link IconSee Also