Modify an Input/Output
- Double-click the cell to edit.
-
-
You can also use the arrow keys to select the cell and press the F2 key to start edition.
- Set its driver name to the one of your choice, for example: CIFDriver (column 3).
- Set its description to the corresponding driver address (column 4).
The Description field format has these characteristics:
- It begins with a “%” character.
- Followed by the type of I/O.
I: input, Q: Output
- Followed by the size of I/O.
X: Boolean (1 bit), B: byte (8 bits), W: word (16 bits), D: double word (32 bits), L: long word (64 bits)
- Followed by its address on the selected bus.
The address has the following format: “deviceId.slaveId.moduleId.bitOffset”, where deviceId, slaveId, moduleId and bitOffset are integers ranging from 0 to 65535.
- set deviceId to 0
- set slaveId to the id of the I/O node
- set moduleId to the id of the slice
- bitOffset must always be 0 for non-Boolean I/Os
-
-
The size of the variable and the I/O must be the same.
Example
%IX0.1.2.4 is an input Boolean located on deviceId=0, slaveId=1, moduleId=2 at bitOffset=4
%QB0.1.2.0 is an output byte located on deviceId=0, slaveId=1, moduleId=2
-
-
If you enter invalid text, the table cell becomes red and an explanation appears in the information column.
See Also