Trace Zoom Feature
Two zoom modes are available:
|
Mode |
Description |
|---|---|
|
Amplitude zoom |
Used to have a better view of a part of a signal. This zoom operation updates the amplitude and zero offset value.
|
|
Time zoom |
Used to expand/collapse the time-base in order to have a better view of the signal evolution through time. This zoom operation updates the time-base value. |
The zoom operations can be done by either:
- Modifying the corresponding values by hand.
- Using the mouse wheel.
See Setting Scale about setting the amplitude, zero offset, and time-base values.
Mouse Shortcuts
|
Result |
|
|---|---|
|
Scroll up the mouse wheel. |
Expands the time-base value. |
|
Scroll down the mouse wheel. |
Collapses the time-base value. |
|
Press the Ctrl key while scrolling up. |
Makes the amplitude value greater. |
|
Press the Ctrl key while scrolling down. |
Makes the amplitude value smaller. |