Web Diagnostic Panels

This section describes how to:

Overview

The Web Diagnostic Panels is used to interact with and manage control panels designed in the KAS-IDE through a browser-based interface.

This feature provides a convenient way to visualize and operate control logic without requiring native applications or additional software installations.

Key Features

  • Browser-Based Access: Control panels can be accessed via standard desktop web browsers.
  • Real-Time Interaction: Users can monitor, and control system parameters live.
  • Custom Panel Layouts: Panels designed in the IDE retain their layout and styling when rendered in the browser.
  • No Installation Required: Runs directly in supported browsers without additional plugins.

Prerequisites

  • The KAS-IDE must be installed on the computer.
  • A project must be configured with the Generate Web-based Control Panels check box selected.
  • The target controller must support web content generation (e.g., PCMM2G).

Overall Procedures

These are the overall steps to configure an application and access the web-based diagnostic panels:

  1. Create and Configure an Application
  2. Access Web Diagnostic Panels in a Browser.