WorkBench Views in the KAS-IDE

WorkBench 2 views are integrated into the KAS-IDE, and are accessible from the Kollmorgen servo drives's Configuration tab when the controller is started or in Online Configuration mode.

The device views for Kollmorgen AKD Series Servo Drives may be different from each other because the devices have different capabilities.


  • To save resources and minimize the time it takes to open a project, the state of the drive's WorkBench views integrated inside the KAS-IDE are not saved.
    Views need to be opened each time a project is opened.