Windows Standard Conventions
Windows Manipulation
These standards apply to the KAS-IDE windows:
- Move
- Resize
- Minimize
- Maximize
- Close (Alt+F4)
Press Esc to exit a pop-up window.
Mouse Manipulation
- Double-click an item to open it (e.g. double-click a program in the Project Explorer to open it in the appropriate editor)
- Right-click to open the menu and give access to the relevant commands (e.g. to add a variable to the Dictionary)
Table Manipulation
Sorting Items
- If the sort feature is implemented, you can click in the column header to sort all the items according to one of the available parameters.
- Click again to alternately sort in ascending or descending order.
Selecting a Cell
- Click a cell in the table to select it.
- Once selected, press F2 to edit the value.
-
-
A double-click directly opens the pop-up window for editing.
Selecting a Row
- When available, press the Spacebar to toggle the selection mode from cell to row.
- Click a cell in the table to select the entire row.
- Once selected, press F2 to edit the values of the row.
Resize a Column
- If you want to enlarge a column width to make more content visible, put the mouse in the table header between two columns so the cursor change to the following
and move right or left to resize your column. - After this operation, you need to scroll horizontally to see the other columns.