ACTION#.CONDITIONVALUE

Description

ACTION#.CONDITIONVALUE defines the value used by ACTION#.CONDITION to test against the source. The range of this keyword depends on the value of ACTION#.SOURCE and ACTION#.CONDITION. Both must be set before setting the condition value. If ACTION#.CONDITION is modified, the range of the ACTION#.CONDITIONVALUE may change, and the value will return to default.

Some conditions do not require a condition value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.SOURCE and ACTION#.CONDITION

Default Value

Depends on ACTION#.SOURCE and ACTION#.CONDITION

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.CONDITIONVALUE

3902h

01h

Signed32

-

1000:1

Read/Write

No

ACTION2.CONDITIONVALUE

3902h

02h

Signed32

-

1000:1

Read/Write

No

ACTION3.CONDITIONVALUE

3902h

03h

Signed32

-

1000:1

Read/Write

No

ACTION4.CONDITIONVALUE

3902h

04h

Signed32

-

1000:1

Read/Write

No

ACTION5.CONDITIONVALUE

3902h

05h

Signed32

-

1000:1

Read/Write

No

ACTION6.CONDITIONVALUE

3902h

06h

Signed32

-

1000:1

Read/Write

No

ACTION7.CONDITIONVALUE

3902h

07h

Signed32

-

1000:1

Read/Write

No

ACTION8.CONDITIONVALUE

3902h

08h

Signed32

-

1000:1

Read/Write

No

ACTION9.CONDITIONVALUE

3902h

09h

Signed32

-

1000:1

Read/Write

No

ACTION10.CONDITIONVALUE

3902h

0ah

Signed32

-

1000:1

Read/Write

No

ACTION11.CONDITIONVALUE

3902h

0bh

Signed32

-

1000:1

Read/Write

No

ACTION12.CONDITIONVALUE

3902h

0ch

Signed32

-

1000:1

Read/Write

No

ACTION13.CONDITIONVALUE

3902h

0dh

Signed32

-

1000:1

Read/Write

No

ACTION14.CONDITIONVALUE

3902h

0eh

Signed32

-

1000:1

Read/Write

No

ACTION15.CONDITIONVALUE

3902h

0fh

Signed32

-

1000:1

Read/Write

No

ACTION16.CONDITIONVALUE

3902h

10h

Signed32

-

1000:1

Read/Write

No

ACTION17.CONDITIONVALUE

3902h

11h

Signed32

-

1000:1

Read/Write

No

ACTION18.CONDITIONVALUE

3902h

12h

Signed32

-

1000:1

Read/Write

No

ACTION19.CONDITIONVALUE

3902h

13h

Signed32

-

1000:1

Read/Write

No

ACTION20.CONDITIONVALUE

3902h

14h

Signed32

-

1000:1

Read/Write

No

ACTION21.CONDITIONVALUE

3902h

15h

Signed32

-

1000:1

Read/Write

No

ACTION22.CONDITIONVALUE

3902h

16h

Signed32

-

1000:1

Read/Write

No

ACTION23.CONDITIONVALUE

3902h

17h

Signed32

-

1000:1

Read/Write

No

ACTION24.CONDITIONVALUE

3902h

18h

Signed32

-

1000:1

Read/Write

No

ACTION25.CONDITIONVALUE

3902h

19h

Signed32

-

1000:1

Read/Write

No

ACTION26.CONDITIONVALUE

3902h

1ah

Signed32

-

1000:1

Read/Write

No

ACTION27.CONDITIONVALUE

3902h

1bh

Signed32

-

1000:1

Read/Write

No

ACTION28.CONDITIONVALUE

3902h

1ch

Signed32

-

1000:1

Read/Write

No

ACTION29.CONDITIONVALUE

3902h

1dh

Signed32

-

1000:1

Read/Write

No

ACTION30.CONDITIONVALUE

3902h

1eh

Signed32

-

1000:1

Read/Write

No

ACTION31.CONDITIONVALUE

3902h

1fh

Signed32

-

1000:1

Read/Write

No

ACTION32.CONDITIONVALUE

3902h

20h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

40300

1

40300 (0x9d6c)

ACTION1.CONDITIONVALUE

Signed32

Read/Write

Yes

40301

1

40301 (0x9d6d)

ACTION2.CONDITIONVALUE

Signed32

Read/Write

Yes

40302

1

40302 (0x9d6e)

ACTION3.CONDITIONVALUE

Signed32

Read/Write

Yes

40303

1

40303 (0x9d6f)

ACTION4.CONDITIONVALUE

Signed32

Read/Write

Yes

40304

1

40304 (0x9d70)

ACTION5.CONDITIONVALUE

Signed32

Read/Write

Yes

40305

1

40305 (0x9d71)

ACTION6.CONDITIONVALUE

Signed32

Read/Write

Yes

40306

1

40306 (0x9d72)

ACTION7.CONDITIONVALUE

Signed32

Read/Write

Yes

40307

1

40307 (0x9d73)

ACTION8.CONDITIONVALUE

Signed32

Read/Write

Yes

40308

1

40308 (0x9d74)

ACTION9.CONDITIONVALUE

Signed32

Read/Write

Yes

40309

1

40309 (0x9d75)

ACTION10.CONDITIONVALUE

Signed32

Read/Write

Yes

40310

1

40310 (0x9d76)

ACTION11.CONDITIONVALUE

Signed32

Read/Write

Yes

40311

1

40311 (0x9d77)

ACTION12.CONDITIONVALUE

Signed32

Read/Write

Yes

40312

1

40312 (0x9d78)

ACTION13.CONDITIONVALUE

Signed32

Read/Write

Yes

40313

1

40313 (0x9d79)

ACTION14.CONDITIONVALUE

Signed32

Read/Write

Yes

40314

1

40314 (0x9d7a)

ACTION15.CONDITIONVALUE

Signed32

Read/Write

Yes

40315

1

40315 (0x9d7b)

ACTION16.CONDITIONVALUE

Signed32

Read/Write

Yes

40316

1

40316 (0x9d7c)

ACTION17.CONDITIONVALUE

Signed32

Read/Write

Yes

40317

1

40317 (0x9d7d)

ACTION18.CONDITIONVALUE

Signed32

Read/Write

Yes

40318

1

40318 (0x9d7e)

ACTION19.CONDITIONVALUE

Signed32

Read/Write

Yes

40319

1

40319 (0x9d7f)

ACTION20.CONDITIONVALUE

Signed32

Read/Write

Yes

40320

1

40320 (0x9d80)

ACTION21.CONDITIONVALUE

Signed32

Read/Write

Yes

40321

1

40321 (0x9d81)

ACTION22.CONDITIONVALUE

Signed32

Read/Write

Yes

40322

1

40322 (0x9d82)

ACTION23.CONDITIONVALUE

Signed32

Read/Write

Yes

40323

1

40323 (0x9d83)

ACTION24.CONDITIONVALUE

Signed32

Read/Write

Yes

40324

1

40324 (0x9d84)

ACTION25.CONDITIONVALUE

Signed32

Read/Write

Yes

40325

1

40325 (0x9d85)

ACTION26.CONDITIONVALUE

Signed32

Read/Write

Yes

40326

1

40326 (0x9d86)

ACTION27.CONDITIONVALUE

Signed32

Read/Write

Yes

40327

1

40327 (0x9d87)

ACTION28.CONDITIONVALUE

Signed32

Read/Write

Yes

40328

1

40328 (0x9d88)

ACTION29.CONDITIONVALUE

Signed32

Read/Write

Yes

40329

1

40329 (0x9d89)

ACTION30.CONDITIONVALUE

Signed32

Read/Write

Yes

40330

1

40330 (0x9d8a)

ACTION31.CONDITIONVALUE

Signed32

Read/Write

Yes

40331

1

40331 (0x9d8b)

ACTION32.CONDITIONVALUE

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.CONDITIONVALUE

40300

Float

Read/Write

-

ACTION2.CONDITIONVALUE

40301

Float

Read/Write

-

ACTION3.CONDITIONVALUE

40302

Float

Read/Write

-

ACTION4.CONDITIONVALUE

40303

Float

Read/Write

-

ACTION5.CONDITIONVALUE

40304

Float

Read/Write

-

ACTION6.CONDITIONVALUE

40305

Float

Read/Write

-

ACTION7.CONDITIONVALUE

40306

Float

Read/Write

-

ACTION8.CONDITIONVALUE

40307

Float

Read/Write

-

ACTION9.CONDITIONVALUE

40308

Float

Read/Write

-

ACTION10.CONDITIONVALUE

40309

Float

Read/Write

-

ACTION11.CONDITIONVALUE

40310

Float

Read/Write

-

ACTION12.CONDITIONVALUE

40311

Float

Read/Write

-

ACTION13.CONDITIONVALUE

40312

Float

Read/Write

-

ACTION14.CONDITIONVALUE

40313

Float

Read/Write

-

ACTION15.CONDITIONVALUE

40314

Float

Read/Write

-

ACTION16.CONDITIONVALUE

40315

Float

Read/Write

-

ACTION17.CONDITIONVALUE

40316

Float

Read/Write

-

ACTION18.CONDITIONVALUE

40317

Float

Read/Write

-

ACTION19.CONDITIONVALUE

40318

Float

Read/Write

-

ACTION20.CONDITIONVALUE

40319

Float

Read/Write

-

ACTION21.CONDITIONVALUE

40320

Float

Read/Write

-

ACTION22.CONDITIONVALUE

40321

Float

Read/Write

-

ACTION23.CONDITIONVALUE

40322

Float

Read/Write

-

ACTION24.CONDITIONVALUE

40323

Float

Read/Write

-

ACTION25.CONDITIONVALUE

40324

Float

Read/Write

-

ACTION26.CONDITIONVALUE

40325

Float

Read/Write

-

ACTION27.CONDITIONVALUE

40326

Float

Read/Write

-

ACTION28.CONDITIONVALUE

40327

Float

Read/Write

-

ACTION29.CONDITIONVALUE

40328

Float

Read/Write

-

ACTION30.CONDITIONVALUE

40329

Float

Read/Write

-

ACTION31.CONDITIONVALUE

40330

Float

Read/Write

-

ACTION32.CONDITIONVALUE

40331

Float

Read/Write

-