AXIS#.TUNING.ISSLIDERINUSE

Description

AXIS#.TUNING.ISSLIDERINUSE indicates whether the current tuning solution was computed by the QuickTune feature or the Slider Tuning feature. This value also indicates if the keyword AXIS#.TUNING.BANDWIDTH is valid or not. If this value is 0, then a Bode measurement is needed to identify the velocity loop bandwidth.

Versions

Action Version Notes
Implemented 02-13-01-000 

-

General Information

Type Read Only
Units N/A
Range 0 - 1
Default Value 1
Data Type Integer
See Also AXIS#.TUNING.BANDWIDTH
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.