DOUT#.STATE

Description

Reads the state of one digital output according to the number identified in the command.

Examples

Code

--> DOUT1.STATE
1

Context

See Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type Read Only
Units N/A
Range 0 to 1
Default Value N/A
Data Type Integer
See Also  

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

21000

1

21000 (0x5208)

DOUT1.STATE

Unsigned8

Read Only

Yes

21001

1

21001 (0x5209)

DOUT2.STATE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DOUT1.STATE

21000

Unsigned8

Read Only

-

DOUT2.STATE

21001

Unsigned8

Read Only

-