REC.OFF

Description

REC.OFF turns the recorder off. In order to set the recorder again, the recorder must first be armed and then a trigger set.

Examples

Code

If a recording is triggered before this command is executed, this command will cancel the recording and the recording state will go to Idle.

-->REC.OFF

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REC.ACTIVE , REC.DONE

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2304

1

2304 (0x900)

REC.OFF

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

REC.OFF

2304

Unsigned8

Read/Write

-