AOUT.VALUE
Description
AOUT.VALUE reads the analog output value.
General Information
|
Type |
R/O Parameter |
|
Units |
V |
|
Range |
–10 to +10 V |
|
Default Value |
0 |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
| Index/Subindex |
|---|
|
3470h/2 |