DRV.DISTO

Description

This timer starts when DRV.DIS is issued (regardless of the DRV.DIS origin). After this timeout elapses, the actual state of the drive is compared to the DRV.DISMODE setting. If the actual state does not match the DRV.DISMODE setting, a fault is reported and the hardware immediately executes the DRV.DISMODE setting (for instance, disable or activate dynamic brake). Setting DRV.DISTO to 0 will disable the timeout.

General Information

Type

R/W Parameter

Units

ms

Range

0 to 120,000 ms

Default Value

1,000 ms

Data Type

U32

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3445h/0

M_01-00-00-000

Related Topics

"Controlled Stop"

DRV.DIS, DRV.DISMODE