IL.KVFF

Description

This parameter sets the gain for the velocity loop feedforward. The nominal feedforward value can be multiplied by this gain value.

This parameter is only used in position mode (DRV.OPMODE = 2).

General Information

Type

R/W

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Float

See Also

IL.FF

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3544h/0

M_01-00-00-000

Related Topics

Current Loop