IL.MFOLDD

Description

IL.MFOLDD sets the maximum time allowed for the motor to remain at peak current before starting to fold towards the motor continuous current. When at motor peak current, IL.MFOLDD is the amount of time before the foldback algorithm starts to reduce the current.

General Information

Type

R/O Parameter

Units

s

Range

0.1 to 2400 s

Default Value

10 s

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes

Related Topics

Current Loop