MOTOR.INERTIA

Description

This parameter sets the motor inertia.


  • When this value is changed, the drive will re-calculate and set all tuning parameters to their defaults. Additionally, a fault will be thrown to inform you that default tuning has been implemented.

General Information

Type

NV Parameter

Units

kgcm² for rotary motors

kg for linear motors

Range

1 to 200,000 kgcm² or kg

Default Value

100 kgcm² or kg

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
35ABh/0 M_01-00-00-000

Related Topics

"Motor View"