MOTOR.LQLL

Description

This parameter is used to configure the motor line-to-line inductance.


  • When this value is changed, the drive will re-calculate and set all tuning parameters to their defaults. Additionally, a fault will be thrown to inform you that default tuning has been implemented.

General Information

Type

NV Parameter

Units

mH

Range

1 to 232 mH

Default Value

17.000 mH

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3455h/0 M_01-00-00-000

Related Topics

"Motor View"