MOTOR.NAME

Description

This parameter is used to set the motor name.

General Information

Type

NV Parameter

Units

N/A

Range

20 chars

Default Value

N/A

Data Type

String

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3899h/0 M_01-19-04-000

Related Topics

Motor View