MOTOR.TBRAKEAPP

Description

This parameter is used to configure the mechanical delay required for the motor brake to close. When disabling the drive with DRV.DISMODE not '0 - Disable axis immediately', the drive will servo to hold position for the time set, allowing the brake to apply.


  • If MOTOR.AUTOSET = 1 and FB1.MEMVER > 0.01, this parameter will be automatically configured for Kollmorgen motors.

General Information

Type

NV Parameter

Units

ms

Range

0 to 1,000 ms

Default Value

75 ms

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
366Eh/0 M_01-00-00-000

Related Topics

"Motor View"