MOTOR.VMAX

Description

This parameter sets the maximum motor mechanical speed. The value 1.2 x MOTOR.VMAX becomes the overall overspeed fault threshold (VL.VFTHRESH) if it is less than the user overspeed fault threshold (VL.THRESH), and for MOTOR.TYPE = 6 if it is less than the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (MOTOR.KE x sqrt(2))).

General Information

Type

NV Parameter

Units

rpm

Range

100 to 40,000 rpm

Default Value

3,000 rpm

Data Type

Integer

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
35A3h/0 M_01-00-00-000

Related Topics

"Motor View" | VL.THRESH | VL.VFTHRESH