VL.CMDU

Description

VL.CMDU sets the user velocity command. When DRV.OPMODE is set to 1 (velocity loop) and DRV.CMDSOURCE is set to 0 (TCP/IP channel), then setting this value when the drive is enabled will cause the drive to rotate at the required velocity.

General Information

Type

R/W Parameter

Units

Depends on UNIT.VROTARY (pg 1) or UNIT.VLINEAR (pg 1)

Rotary: rpm, rps, deg/s, custom units/s, rad/s

Linear: counts/s, mm/s, µm/s, custom units/s

Range

Rotary

-15,000.000 to 15,000.000 rpm

-250.000 to 250.000 rps

-90000.000 to 90000.000 deg/s

-1250.000 to 1250.000 custom units/s

-1570.796 to 1570.796 rad/s

Linear

-1,073,741,824,000.000 to 1,073,741,824,000.000 counts/s

-8,000.000 to 8,000.000 mm/s

-8,000,000.000 to 8,000,000.000 µm/s

-1,250.000 to 1,250.000 custom units/s

Default Value

0

Data Type

Float

See Also

VL.FB, VL.CMD, DRV.OPMODE, DRV.CMDSOURCE, VL.LIMITN, VL.LIMITP

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
60FFh/0 M_01-00-00-000

Related Topics

"Velocity Loop"