AXIS#.BODE.CHIRP.ENDFREQ
Description
AXIS#.BODE.CHIRP.ENDFREQ sets the ending frequency for the chirp excitation.
Example
Setting up a chirp excitation source of 0.2 A from 0.1 Hz to 1000 Hz over a period of 1 second:
--> AXIS1.BODE.INJECTPOINT 1 --> AXIS1.BODE.IAMP 0.2 --> AXIS1.BODE.CHIRP.STARTFREQ 0.1 --> AXIS1.BODE.CHIRP.ENDFREQ 1000 --> AXIS1.BODE.CHIRP.TIME 1 --> AXIS1.BODE.MODE 6
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-09-04-000 |
General Information
|
Type |
Read/Write |
|
Description |
Sets the end frequency of the chirp excitation. |
| Units | Hz |
|
Range |
0.1 to 8,000 Hz |
|
Default Value |
1000 Hz |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.