AXIS#.IL​.FOLDFTHRESHU

Description

AXIS#.IL.FOLDFTHRESHU is set by the user as the fault threshold of both motor and drive foldback algorithms. The actual threshold value, namely AXIS#.IL​.FOLDFTHRESH , is the minimum of AXIS#.IL.FOLDFTHRESHU, AXIS#.IPEAK and AXIS#.MOTOR.IPEAK . Setting AXIS#.IL​.FOLDFTHRESHU to zero will stop faults F2001 and F2017 from being generated.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0 to 500 Arms

Default Value

Drive peak current (IPEAK)

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.FOLDFTHRESHU

500ah

09h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5806

1

5806 (0x16ae)

AXIS1.IL.FOLDFTHRESHU

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.FOLDFTHRESHU

5806

Float

Read/Write

-