AXIS#.MOTOR.TEMP
Description
This parameter returns the motor temperature, which is represented as the resistance of the motor's PTC or NTC.
Context
For more information see Motor and Motor Temperature View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Ω |
|
Range |
0 to 232 Ω |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.TEMP |
500bh |
02h |
Unsigned32 |
- |
- |
Read only |
Yes |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6217 |
1 |
6217 (0x1849) |
AXIS1.MOTOR.TEMP |
Unsigned32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.MOTOR.TEMP |
6217 |
Unsigned32 |
Read Only |
- |