AXIS#.PL.KFB.POUT
Please refer to AXIS#.PL.KFB.PIN for details.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-08-01-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 1 to 2,147,483,647 |
| Default Value | 1 |
| Data Type | Integer |
| See Also | AXIS#.PL.KFB, AXIS#.PL.KFB.PIN, AXIS#.VL.KFB |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.PL.KFB.POUT |
500ch |
12h |
Signed32 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5919 |
1 |
5919 (0x171f) |
AXIS1.PL.KFB.POUT |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.PL.KFB.POUT |
5919 |
Signed32 |
Read/Write |
- |