CMP#.WIDTHTYPE
Description
CMP#.WIDTHTYPE sets the type of duration of the output pulse generated by the setpoint. The duration can be either a value in the same units as CMP#.VAL or a time in ms.
It takes two command line arguments: the first specifies the setpoint, and the second specifies the duration type.
Examples
Usage
0: Value in CMP#.SOURCE units (default)
1: Time in ms
Code
These commands set the duration for channel 1 setpoint 2 to value type, and channel 2 setpoint 7 to time type
--> CMP1.WIDTHTYPE 2 0
--> CMP2.WIDTHTYPE 7 1
Context
See Compare Engines View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-06-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
31480 |
1 |
31480 (0x7af8) |
CMP1.WIDTHTYPE |
Unsigned8[8] |
Read/Write |
Yes |
|
31481 |
1 |
31481 (0x7af9) |
CMP2.WIDTHTYPE |
Unsigned8[8] |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CMP1.WIDTHTYPE |
31480 |
Unsigned8[8] |
Read/Write |
- |
|
CMP2.WIDTHTYPE |
31481 |
Unsigned8[8] |
Read/Write |
- |