Description
Sets or gets the polarity of a digital input.
|
Value |
Description |
|---|---|
| 0 – Active High | The digital input state is 1 when voltage is applied to the I/O pin |
| 1 – Active Low | The digital input state is 1 when voltage is removed from the I/O pin |
Examples
Code
With 24VDC on DIN1:
--> DIN1.INV 0 //Active High
--> DIN1.STATE 1 --> DIN1.INV 1 //Active low --> DIN1.STATE 0
With 0V on DIN1:
--> DIN1.INV 0 //Active High
--> DIN1.STATE 0 --> DIN1.INV 1 //Active low --> DIN1.STATE 1
Context
See Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
|
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 (Active high) |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DIN1.INV |
3590h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIN2.INV |
3591h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIN3.INV |
3592h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIN4.INV |
3593h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
20050 |
1 |
20050 (0x4e52) |
DIN1.INV |
Unsigned8 |
Read/Write |
Yes |
|
20051 |
1 |
20051 (0x4e53) |
DIN2.INV |
Unsigned8 |
Read/Write |
Yes |
|
20052 |
1 |
20052 (0x4e54) |
DIN3.INV |
Unsigned8 |
Read/Write |
Yes |
|
20053 |
1 |
20053 (0x4e55) |
DIN4.INV |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DIN1.INV |
20050 |
Unsigned8 |
Read/Write |
- |
|
DIN2.INV |
20051 |
Unsigned8 |
Read/Write |
- |
|
DIN3.INV |
20052 |
Unsigned8 |
Read/Write |
- |
|
DIN4.INV |
20053 |
Unsigned8 |
Read/Write |
- |