Description

Reads the state of one digital input according to the number identified in the command.

Examples

Code

--> DIN1.STATE
1

Context

See Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type Read Only
Units N/A
Range 0 to 1
Default Value N/A
Data Type Integer
See Also  

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

20000

1

20000 (0x4e20)

DIN1.STATE

Unsigned8

Read Only

Yes

20001

1

20001 (0x4e21)

DIN2.STATE

Unsigned8

Read Only

Yes

20002

1

20002 (0x4e22)

DIN3.STATE

Unsigned8

Read Only

Yes

20003

1

20003 (0x4e23)

DIN4.STATE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DIN1.STATE

20000

Unsigned8

Read Only

-

DIN2.STATE

20001

Unsigned8

Read Only

-

DIN3.STATE

20002

Unsigned8

Read Only

-

DIN4.STATE

20003

Unsigned8

Read Only

-