DIO#.SOURCEID
Description
DIO#.SOURCEID sets the digital I/O source ID, for sources that require an ID.
Examples
Usage
DIO#.SOURCEID can be used to select the compare channel whenDIO#.SOURCE = 4 (Compare).
Code
The following commands set the source of digital IO 1 to compare channel 1, and digital IO 2 to compare channel 2.
--> DIO1.SOURCE 4
--> DIO1.SOURCEID 1
--> DIO2.SOURCE 4
--> DIO2.SOURCEID 2
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Added Compare source | 02-06-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 1 to 2 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DIO1.SOURCEID |
368ah |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO2.SOURCEID |
368bh |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO3.SOURCEID |
368ch |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO4.SOURCEID |
368dh |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO5.SOURCEID |
368eh |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO6.SOURCEID |
368fh |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
22300 |
1 |
22300 (0x571c) |
DIO1.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
22301 |
1 |
22301 (0x571d) |
DIO2.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
22302 |
1 |
22302 (0x571e) |
DIO3.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
22303 |
1 |
22303 (0x571f) |
DIO4.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
22304 |
1 |
22304 (0x5720) |
DIO5.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
22305 |
1 |
22305 (0x5721) |
DIO6.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DIO1.SOURCEID |
22300 |
Unsigned8 |
Read/Write |
- |
|
DIO2.SOURCEID |
22301 |
Unsigned8 |
Read/Write |
- |
|
DIO3.SOURCEID |
22302 |
Unsigned8 |
Read/Write |
- |
|
DIO4.SOURCEID |
22303 |
Unsigned8 |
Read/Write |
- |
|
DIO5.SOURCEID |
22304 |
Unsigned8 |
Read/Write |
- |
|
DIO6.SOURCEID |
22305 |
Unsigned8 |
Read/Write |
- |