FB#.LINEPITCH

Description

This parameter defines the line pitch for linear encoders in nm per line. This is only used when using linear motor types. For rotary motors, see FB.ENCLINES.

Context

See Feedback # View and FB#.MECHTYPE.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

nm/line

Range

0.001 to 2000000.000

Default Value

20,000

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB2.LINEPITCH

3501h

0ah

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30381

1

30381 (0x76ad)

FB2.LINEPITCH

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB2.LINEPITCH

30381

Float

Read/Write

-