MW.WARNINGS
Any time a MechaWare warning is issued (most likely Warning 3101) additional details will be available in MW.WARNINGS. The most likely causes of warnings are a misconfiguration of a block or keyword, or something in a custom MechaWare model.
Example
Disable Model 1:
-->MW.MODEL1.STATE 0
This disables the factory model and will not allow the axis to work. This generates Warning 3102. Because this is a MechaWare warning, additional details are available in MW.WARNINGS
-->MW.WARNINGS
Axis: 1, Missing Output Block: Torque Output
This tells us exactly what triggered the warning.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-12-00-000 |
General Information
| Type | Read Only |
| Description | Retrieve verbose warning information about MechaWare related warnings |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | String |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.