PWM#.DUTYCYCLE
Description
Sets the duty cycle of the PWM signal, that can be output on a digital IO with DIO#.SOURCE 6.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-11-03-000 |
General Information
| Type | Read/Write |
| Units | Percent |
| Range | 0.0 to 100.0 |
| Default Value | 0.0 |
| Data Type | Float |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
PWM1.DUTYCYCLE |
38f0h |
02h |
Unsigned32 |
- |
1000:1 |
Read/Write |
Yes |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
42100 |
1 |
42100 (0xa474) |
PWM1.DUTYCYCLE |
Unsigned32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
PWM1.DUTYCYCLE |
42100 |
Float |
Read/Write |
- |