Use ST Expressions in Graphic Language
- This feature makes it possible to simplify FFLD and FBD diagrams when a trivial calculation has to be entered.
- It also enables you to use graphic features for representing a main algorithm as text is used for details of implementation.
- Expression must be written in Structured Text (ST) language.
- An expression is anything you can imagine between parentheses in an ST program.
- The ST expression must fit the data type required by the diagram (e.g., an expression put on a contact must be Boolean).
FBD Language Example
A complex ST expression can be entered in any variable box of an FBD diagram if the box is not connected on its input.
FFLD Language Example
A complex ST expression can be entered on any kind of contact and on any input of a function or function block.